What Are Knobs? Functions, Types, Features, Applications and MoreDescription of Machine elements for Designers Knobs Edition page. We introduce here what knobs are, the advantages of their use, various usage examples, and their types and characteristics.May. 12. 2025 time >
Description of Machine elements for Designers Knobs Edition page. We introduce here what knobs are, the advantages of their use, various usage examples, and their types and characteristics.
May. 12. 2025 time >
Hexagon Socket Head Cap Screws Excerpts from ISO 4762:2004, JIS B 1176:2015 This page describes JIS B 1176 "Hexagon socket head cap screws".Apr. 30. 2025 time >
This page describes JIS B 1176 "Hexagon socket head cap screws".
Apr. 30. 2025 time >
Description of Plungers for EngineersDescription of Machine elements for Designers Plungers Edition page. Plungers are machine elements for positioning and fixing workpieces. We offer a clear introduction to plungers, the advantages of their use, various usage examples, and their types and characteristics.Apr. 30. 2025 time >
Description of Machine elements for Designers Plungers Edition page. Plungers are machine elements for positioning and fixing workpieces. We offer a clear introduction to plungers, the advantages of their use, various usage examples, and their types and characteristics.
Vol. 12 Back to Basics Series! Screw Reference DimensionsThe absolute ABCs, screw reference dimensions that are important when designing. A lot of problems can occur if you use the wrong dimensions when designing or placing an order. Nedzigon will explain screw terminology and use pictures to introduce the various thread types. Apr. 30. 2025 time >
The absolute ABCs, screw reference dimensions that are important when designing. A lot of problems can occur if you use the wrong dimensions when designing or placing an order.
Nedzigon will explain screw terminology and use pictures to introduce the various thread types.
Washers: Essential Components for Secure Connections This page introduces washers. As well as a description of washers, the washer products handled by NBK are introduced. Apr. 23. 2025 time >
This page introduces washers. As well as a description of washers, the washer products handled by NBK are introduced.
Apr. 23. 2025 time >
CE-marked components which prevent foreign matter contamination are required 【Safety / precautionary measures】Introducing components with a captive mechanism.Mar. 25. 2025 time >
Introducing components with a captive mechanism.
Mar. 25. 2025 time >
Only certain workersshould be able to remove screws 【Safety Measures/Precautionary Measures】Introducing screws requiring dedicated tools for removal.Mar. 12. 2025 time >
Introducing screws requiring dedicated tools for removal.
Mar. 12. 2025 time >
Products conforming to SEMI standards are required【Safety Measures/Precautionary Measures】Introducing our abundant lineup of SEMI standard compliant products.Mar. 12. 2025 time >
Introducing our abundant lineup of SEMI standard compliant products.
CE marking compliance is required【Workability/Maintenance】Introducing screws which don't fall out when the cover is removed.Mar. 11. 2025 time >
Introducing screws which don't fall out when the cover is removed.
Mar. 11. 2025 time >
Monitors need to be movable with one touch in accordance with the worker's height or the nature of the work【Improved productivity/workability】Introducing parts enabling free adjustment of the monitor position.Mar. 10. 2025 time >
Introducing parts enabling free adjustment of the monitor position.
Mar. 10. 2025 time >
Washer fall-out prevention is required 【Workability/Maintenance】Introducing integrated washer type screws.Feb. 27. 2025 time >
Introducing integrated washer type screws.
Feb. 27. 2025 time >
No. 5: Solving common problems inside equipmentIn Part 5, we will introduce NBK products used in semiconductor manufacturing equipment interiors, as well as various examples of the resolution of issues such as vacuum, heat-resistance, isolation and so on. Feb. 17. 2025 time >
In Part 5, we will introduce NBK products used in semiconductor manufacturing equipment interiors, as well as various examples of the resolution of issues such as vacuum, heat-resistance, isolation and so on.
Feb. 17. 2025 time >
Screws that will not affect communication are required 【Safety Measures/Precautionary Measures】Introducing plastic screws that will not affect communication.Feb. 14. 2025 time >
Introducing plastic screws that will not affect communication.
Feb. 14. 2025 time >
About SUH660SUH660 is austenitic heat-resistant steel. With high strength at high temperatures, it can be used in environments up to 700°CJan. 28. 2025 time >
SUH660 is austenitic heat-resistant steel. With high strength at high temperatures, it can be used in environments up to 700°C
Jan. 28. 2025 time >
General TolerancesThis page describes JIS B 0405 / JIS B 0419 "General tolerances".Jan. 27. 2025 time >
This page describes JIS B 0405 / JIS B 0419 "General tolerances".
Jan. 27. 2025 time >
Hexagon NutsThis page describes JIS B 1181 "Hexagon Nuts (those not dependent on ISO 4032 to 4036 and ISO 8673 to 8675)".Jan. 27. 2025 time >
This page describes JIS B 1181 "Hexagon Nuts (those not dependent on ISO 4032 to 4036 and ISO 8673 to 8675)".
NEW SAVE