No. 2: Vacuum environmentsVacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments! Dec. 05. 2025 time >
Vacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments!
Dec. 05. 2025 time >
Description of Tamper Resistant Screws for the EngineersThis is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.Nov. 25. 2025 time >
This is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.
Nov. 25. 2025 time >
Galling and SeizingThis is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.Nov. 25. 2025 time >
This is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.
Micro Screws: M0.6 (S0.6) to M2.6 LineupNBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space. Nov. 25. 2025 time >
NBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space.
No. 6: Thermal CyclingHere we discuss thermal cycling, which is often an issue in semiconductor manufacturing equipment. Nov. 25. 2025 time >
Here we discuss thermal cycling, which is often an issue in semiconductor manufacturing equipment.
Miniature Screws/Precision Screws Lineup ListThis is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.Nov. 25. 2025 time >
This is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.
What are Hex Socket Head Cap Screws (cap bolts)? Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc. Nov. 25. 2025 time >
Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc.
Special Surface Hardened ScrewsSpecial Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.Nov. 25. 2025 time >
Special Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.
Increased degree of vacuum in equipment is required 【Productivity increase】Introducing screws which support use with vacuum equipment.Nov. 25. 2025 time >
Introducing screws which support use with vacuum equipment.
Select the best screws for your needsThis page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etcNov. 25. 2025 time >
This page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc
No. 1: The Semiconductor Industry and NBKAlong with the dramatic worldwide growth of semiconductors, similar development has taken place for semiconductor manufacturing equipment. For many years, NBK has developed and sold products for semiconductor manufacturing equipment.In Part 1, we introduce trends in the semiconductor industry, and describe some interesting efforts by NBK! Nov. 25. 2025 time >
Along with the dramatic worldwide growth of semiconductors, similar development has taken place for semiconductor manufacturing equipment. For many years, NBK has developed and sold products for semiconductor manufacturing equipment.In Part 1, we introduce trends in the semiconductor industry, and describe some interesting efforts by NBK!
What is a Coupling? Explanation of Types and CharacteristicsA coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.Nov. 12. 2025 time >
A coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.
Nov. 12. 2025 time >
Select Based on ApplicationSelect Coupling based on application Nov. 10. 2025 time >
Select Coupling based on application
Nov. 10. 2025 time >
Points to Consider When Mounting DisplaysWe describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.Oct. 29. 2025 time >
We describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.
Oct. 29. 2025 time >
RoHS compatible all-stainless steel couplings are required 【High sanitation / corrosion-resistant / clean】Our abundant lineup allows us to ship highly reliable products with short lead times.Oct. 29. 2025 time >
Our abundant lineup allows us to ship highly reliable products with short lead times.
Screws in places unreachable by hand need to be tightened 【Workability / maintenance】Introducing a product for holding screws with excellent workability.Oct. 29. 2025 time >
Introducing a product for holding screws with excellent workability.
NEW SAVE