Screws with high strength are required even in environments where steel cannot be used 【Compact / lightweight】Introducing screws using stainless steel/titanium screws with strength equivalent to steel for space and weight saving.May. 14. 2020 time >
Introducing screws using stainless steel/titanium screws with strength equivalent to steel for space and weight saving.
May. 14. 2020 time >
Vibration of the machine must be prevented to maintain workpiece machining accuracy 【Productivity increase】Introducing case studies using couplings with high torsional stiffness and vibration absorption functions to improve productivity.May. 10. 2020 time >
Introducing case studies using couplings with high torsional stiffness and vibration absorption functions to improve productivity.
May. 10. 2020 time >
Disturbances / vibrations must be suppressed 【Safety / precautionary measures】Introducing case studies using couplings that suppress vibrations to prevent disturbances/vibrations.May. 10. 2020 time >
Introducing case studies using couplings that suppress vibrations to prevent disturbances/vibrations.
Couplings that support minimal outgassing and large eccentricity are required 【High sanitation / corrosion-resistant / clean】Introducing Oldham couplings using PEEK spacers to support clean/vacuum environments with heat resistance.May. 10. 2020 time >
Introducing Oldham couplings using PEEK spacers to support clean/vacuum environments with heat resistance.
Stable speed control of the raising / lowering shaft is required 【High rigidity / high accuracy】Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.May. 10. 2020 time >
Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.
Long actuator hunting must be suppressed 【Automation / robots / motorization】Couplings with superior damping performance can be used to suppress hunting and enable highly responsive transport.May. 10. 2020 time >
Couplings with superior damping performance can be used to suppress hunting and enable highly responsive transport.
Improved coupling insulation properties are required 【Compact / lightweight】Introducing case studies using PEEK couplings with good insulation properties to shrink and reduce the weight of machinery.May. 10. 2020 time >
Introducing case studies using PEEK couplings with good insulation properties to shrink and reduce the weight of machinery.
Shaft fastening time must be reduced 【Workability / maintenance】Introducing case studies using split type couplings to reduce shaft fastening time. May. 10. 2020 time >
Introducing case studies using split type couplings to reduce shaft fastening time.
350% instantaneous maximum torque needs to be handled 【Compact / lightweight】Introducing case studies where high-rigidity couplings are used to improve torque transmission.May. 10. 2020 time >
Introducing case studies where high-rigidity couplings are used to improve torque transmission.
Coupling maintenance frequency must be drastically reduced 【Workability / maintenance】High torque and long-term maintenance free coupling for improving machine reliability. May. 10. 2020 time >
High torque and long-term maintenance free coupling for improving machine reliability.
Tablet PCs must be fixed to equipment 【Workability / maintenance】Introducing products for easily fixing tablet PCs to equipment using magnets. May. 10. 2020 time >
Introducing products for easily fixing tablet PCs to equipment using magnets.
LCD monitors/tablets must be fixed to equipment 【Elegant functionality / design】Introducing display mounting components specialized for production sites. May. 10. 2020 time >
Introducing display mounting components specialized for production sites.
Solving common issues with Semiconductor Manufacturing Equipment(Post-Process)This section introduces countermeasures for the special environments necessary for semiconductor manufacturing equipment (post-process), and measures to improve productivity.May. 10. 2020 time >
This section introduces countermeasures for the special environments necessary for semiconductor manufacturing equipment (post-process), and measures to improve productivity.
Simpler cleanroom support is required 【High sanitation / corrosion-resistant / clean】Introducing cleanroom wash/cleanroom packaging service.May. 10. 2020 time >
Introducing cleanroom wash/cleanroom packaging service.
Screw corrosion prevention is required in environments subjected to water 【High sanitation / corrosion-resistant / clean】Introducing screws that prevents galvanic corrosion.May. 10. 2020 time >
Introducing screws that prevents galvanic corrosion.
Corrosion countermeasures for salt water are required for screws 【High sanitation / corrosion-resistant / clean】Introducing two-phase stainless steel screws with strength and corrosion resistance superior to SUS316L.May. 10. 2020 time >
Introducing two-phase stainless steel screws with strength and corrosion resistance superior to SUS316L.
NEW SAVE