Date Published:Aug. 03. 2018
Using the Clamp Lever / Tension Lever
Using the Clamp Lever / Tension Lever
| Clamp Lever Miniature Clamp Lever |
Clamp Lever (Double Arm Type) |
Tension Lever | |
|---|---|---|---|
| ❶Pull up the lever. The built-in spring will be compressed and the engaged serrations will be disengaged. |
![]() |
![]() |
![]() |
| ❷Next, turn the freed lever to the desired position. |
![]() |
![]() |
![]() |
| ❸Release the lever to retract it with the spring force, re-engage the serrations, and lock it. |
![]() |
![]() |
![]() |
Definitions of Max. Load and Max. Tightening Force
● Clamp Lever
Miniature Clamp Lever

● Clamp Lever
(Double Arm Type)

● Tension Lever

Only takes a minute to understand! How to Use Clamp Levers.
Usage
Others
Machine Tools
Semiconductor Manufacturing Equipment
Food Machinery
Automotive Manufacturing Process
Medical equipment
FA Devices
Machine Elements