Date Published:Sep. 06. 2024
Moving the control panel of a machine tool horizontally【Workability & Maintenance】
There are units available that rotate the control panel horizontally.
By adjusting the control panel to an easy-to-see angle, work efficiency can be improved.▶You can pass the control panel wiring through the central hole of the swivel unit.


Recommended Products
Swivel Mount DKSF
Issue/case studies
Installation Method/Maintenance
Solution samples
Machine Elements