Date Published:May. 10. 2020
Improvement points for FA Devices【Drive Design】
Introducing points for improvement of the performance of the drive design of transport devices, packaging machinery, etc.

Hunting countermeasures for operation with high servomotor gain
Couplings with excellent damping performance should be used▶
Couplings with excellent damping performance should be used(Long actuator)▶
High torque transmission/high-precision positioning
High-rigidity couplings should be used to improve torque transmission▶
High rigidity disk couplings should be used▶
Drive control in vacuum environments
PEEK couplings with good insulation properties should be used▶
PEEK spacer type Oldham couplings are ideal▶
Highly sanitary, corrosion-resistant properties needed
We have an inventory of RoHS compliant couplings▶
Countermeasures for large misalignment
High-torque, long-term maintenance free metal spacer types should be used▶
Issue/case studies
Improved productivity/workability
Safety measures/precautionary measures
Vibration prevention/high precision
Heat resistance/corrosion resistance
Cleanroom/vacuum/non-magnetic
FA Devices
Solution samples
Couplings