Date Published:May. 10. 2020
Removing stripped screws 【Workability / maintenance】
Dedicated tools for removing damaged screws are available
There are special tools for removing damaged hex bolts and hex nuts or stripped screws that cannot be removed with ordinary tools. Screws can be easily removed with this tool even when the corners or recesses of the head have been stripped due to using a shallow tool or the wrong size tool.
●Stripped Screw Removal Bits
Creates grooves in the damaged recesses which can be used to turn and remove the screw.
●Stripped Hex Head Screws/bolts Removal Sockets
The spiral edges inside the socket firmly bite into the socket to enable removal.
Recommended product
Damaged Screw Removal Tool SKEID
Issue/case studies
Improved productivity/workability
Machine Tools
Semiconductor Manufacturing Equipment
Food Machinery
Automotive Manufacturing Process
Medical equipment
FA Devices
Solution samples
Special Screws