Remote Gauge Inspection Cameras
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
SEMI Standard (SEMI S8-0218)Compliant Products
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
Nov. 07. 2023
Nov. 10. 2025
Nov. 26. 2025
Oct. 28. 2025
Jun. 24. 2025
May. 15. 2025
Apr. 30. 2025
Jun. 28. 2024
Jan. 29. 2024
Jan. 19. 2024
Sep. 05. 2025
Oct. 25. 2016
Sep. 23. 2016
Jan. 06. 2015
Nov. 12. 2025
Oct. 29. 2025
Dec. 02. 2024
Oct. 07. 2024
Mar. 26. 2024
Nov. 18. 2024
Jan. 14. 2025
Feb. 17. 2025
May. 16. 2025
Jan. 10. 2025
May. 12. 2025
Nov. 28. 2024
Nov. 06. 2024
May. 28. 2024
Dec. 22. 2025
Dec. 16. 2024
Nov. 27. 2024
Nov. 01. 2024
No. 2: Vacuum environmentsVacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments! Dec. 05. 2025 time >
Vacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments!
Dec. 05. 2025 time >
Description of Tamper Resistant Screws for the EngineersThis is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.Nov. 25. 2025 time >
This is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.
Nov. 25. 2025 time >
Galling and SeizingThis is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.Nov. 25. 2025 time >
This is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.
Micro Screws: M0.6 (S0.6) to M2.6 LineupNBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space. Nov. 25. 2025 time >
NBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space.
Miniature Screws/Precision Screws Lineup ListThis is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.Nov. 25. 2025 time >
This is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.
What are Hex Socket Head Cap Screws (cap bolts)? Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc. Nov. 25. 2025 time >
Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc.
Special Surface Hardened ScrewsSpecial Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.Nov. 25. 2025 time >
Special Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.
Select the best screws for your needsThis page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etcNov. 25. 2025 time >
This page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc
What is a Coupling? Explanation of Types and CharacteristicsA coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.Nov. 12. 2025 time >
A coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.
Nov. 12. 2025 time >
Select Based on ApplicationSelect Coupling based on application Nov. 10. 2025 time >
Select Coupling based on application
Nov. 10. 2025 time >
Points to Consider When Mounting DisplaysWe describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.Oct. 29. 2025 time >
We describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.
Oct. 29. 2025 time >
Screws in places unreachable by hand need to be tightened 【Workability / maintenance】Introducing a product for holding screws with excellent workability.Oct. 29. 2025 time >
Introducing a product for holding screws with excellent workability.
What are Hex Nuts?Here we offer a clear introduction to hex nuts.Oct. 29. 2025 time >
Here we offer a clear introduction to hex nuts.
Theft Prevention NutsNBK's theft prevention nut can prevent crime in various structures without compromising the workability of mounting.Oct. 29. 2025 time >
NBK's theft prevention nut can prevent crime in various structures without compromising the workability of mounting.
Theft / tampering countermeasures are required 【Safety / precautionary measures】Introducing case studies using components that cannot be removed with commercially available tools for use as theft/tampering countermeasures.Oct. 29. 2025 time >
Introducing case studies using components that cannot be removed with commercially available tools for use as theft/tampering countermeasures.
RoHS compatible all-stainless steel couplings are required 【High sanitation / corrosion-resistant / clean】Our abundant lineup allows us to ship highly reliable products with short lead times.Oct. 29. 2025 time >
Our abundant lineup allows us to ship highly reliable products with short lead times.
NEW SAVE