Nov. 08. 2023
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
Jan. 09. 2025
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
Apr. 08. 2024
Stable speed control of the raising / lowering shaft is required 【High rigidity / high accuracy】Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.May. 10. 2020 time >
Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.
May. 10. 2020 time >
Long actuator hunting must be suppressed 【Automation / robots / motorization】Couplings with superior damping performance can be used to suppress hunting and enable highly responsive transport.May. 10. 2020 time >
Couplings with superior damping performance can be used to suppress hunting and enable highly responsive transport.
Shaft fastening time must be reduced 【Workability / maintenance】Introducing case studies using split type couplings to reduce shaft fastening time. May. 10. 2020 time >
Introducing case studies using split type couplings to reduce shaft fastening time.
350% instantaneous maximum torque needs to be handled 【Compact / lightweight】Introducing case studies where high-rigidity couplings are used to improve torque transmission.May. 10. 2020 time >
Introducing case studies where high-rigidity couplings are used to improve torque transmission.
Coupling maintenance frequency must be drastically reduced 【Workability / maintenance】High torque and long-term maintenance free coupling for improving machine reliability. May. 10. 2020 time >
High torque and long-term maintenance free coupling for improving machine reliability.
Tablet PCs must be fixed to equipment 【Workability / maintenance】Introducing products for easily fixing tablet PCs to equipment using magnets. May. 10. 2020 time >
Introducing products for easily fixing tablet PCs to equipment using magnets.
LCD monitors/tablets must be fixed to equipment 【Elegant functionality / design】Introducing display mounting components specialized for production sites. May. 10. 2020 time >
Introducing display mounting components specialized for production sites.
Simpler cleanroom support is required 【High sanitation / corrosion-resistant / clean】Introducing cleanroom wash/cleanroom packaging service.May. 10. 2020 time >
Introducing cleanroom wash/cleanroom packaging service.
Solving common issues with Machine Tools(Machining Center)Introducing improvements to precision and countermeasures for emergencies as required when designing machining centers.May. 10. 2020 time >
Introducing improvements to precision and countermeasures for emergencies as required when designing machining centers.
Solving common issues with Machine Tools(Lathe / Multi-tasking Machine)Introducing improvements to precision and countermeasures for emergencies as required when designing lathes and composite machine tools.May. 10. 2020 time >
Introducing improvements to precision and countermeasures for emergencies as required when designing lathes and composite machine tools.
Screw corrosion prevention is required in environments subjected to water 【High sanitation / corrosion-resistant / clean】Introducing screws that prevents galvanic corrosion.May. 10. 2020 time >
Introducing screws that prevents galvanic corrosion.
Corrosion countermeasures for salt water are required for screws 【High sanitation / corrosion-resistant / clean】Introducing two-phase stainless steel screws with strength and corrosion resistance superior to SUS316L.May. 10. 2020 time >
Introducing two-phase stainless steel screws with strength and corrosion resistance superior to SUS316L.
Tools that can be used even in narrow working spaces are required 【Workability / maintenance】Introducing tools especially for improving workability in narrow spaces.May. 10. 2020 time >
Introducing tools especially for improving workability in narrow spaces.
Screws that can be used in limited spaces are required 【Elegant functionality / design】Introducing case studies in which the ultra-thin head beautifully decorates the mounting surface.May. 10. 2020 time >
Introducing case studies in which the ultra-thin head beautifully decorates the mounting surface.
Countermeasures for screw loosening are required 【Safety / precautionary measures】Introducing washers that prevent screw loosening simply by combining with commercially available hex nuts.May. 10. 2020 time >
Introducing washers that prevent screw loosening simply by combining with commercially available hex nuts.
Screws that retain high strength even in high-temperature environments are required 【Productivity increase】Introducing screws with excellent heat resistance.May. 10. 2020 time >
Introducing screws with excellent heat resistance.
NEW SAVE