Date Published:May. 10. 2020
Improvement points for FA Devices【Unit Design】
Introducing points for improvement of the performance of the modular design of transport devices, packaging machinery, etc.

The time taking setting up workpieces on the line needs to be reduced
*Wireless Positioning Units is sold only in the following countries and regions.
USA, Canada, Korea, Taiwan
Instead of operating handles, equipment with automatic positioning capability is available▶
Special screws that can be used in vacuum/ high temperature/chemical environments
Screws which support equipment vacuuming are in stock▶
Screws with excellent heat resistance are in stock▶
Screws with excellent chemical resistance and screws with head coating only are available▶
Countermeasures when available space is limited
Tools optimized for working in narrow spaces are available▶
Issue/case studies
Improved productivity/workability
Safety measures/precautionary measures
Reduced cost/energy saving/long life
Compact/space-saving/lightweight
High strength/high rigidity
Automation/robots/motorization
FA Devices
Solution samples
Special Screws
FA solutions